As hydrogen fuel cell use becomes more commonplace, Parker remains committed to the safe deployment of hydrogen as an alternative fuel source. To do so, we offer a wide range of EC-79 Certified components for hydrogen Fuel Cell Electric Vehicles (FCEV) fuel systems, buses, marine applications. Components for on-board hydrogen powered vehicles for pressures from 30 to 700 bar (435 to 10,152 psi)
With more than 10,000 alternative fueling stations globally – and more than a dozen alternative fuels in production or under development – consumers and industry together are clamoring for a clean energy future. Parker's Instrumentation Products Division can engineer and manufacture ISO 19880-3 Certified components for hydrogen refueling stations for pressures up to 700 bar (10,152 psi)
Fluid conveyance on a green hydrogen electrolyser refers to the system of fittings, valves, and tubing used to transfer fluids, such as water and electrolyte, to and from the electrolyser cells. Parker’s products are designed to handle the pressures from vacuum to 1,380 bar (20,000 psi) and temperatures required for the electrolysis process. and are manufactured in a range of corrosion-resistant alloys.
Parker’s Bestobell cryogenic valves are specifically designed to be used in cryogenic applications where extremely low temperatures are present. These valves are commonly used in the transportation of liquefied gases, including hydrogen, which must be kept at temperatures well below their boiling points to remain in their liquid form. When transporting hydrogen, the use of Bestobell cryogenic valves is important to ensure the safety and efficiency of the transport process.
Supercritical
Discover how Parker collaborated with hydrogen equipment manufacturer SUPERCRITICAL and helped them bring their first-of-its-kind, zero-emission, ultra-efficient, and iridium-free green hydrogen generator to market, during the most globally challenging economic environment in decades.
ULEMCo
The use of Parker EC-79 rated fittings for hydrogen applications, alongside close collaboration with OEM ULEMCo and a Parker Partner, is helping to pioneer technology that allows commercial vehicle fleet owners to include hydrogen among their running fuels. Taking advantage of zero-emission hydrogen fuel supports wider strategies to reduce transport-related carbon footprint.
As a source of clean energy, hydrogen is making a great contribution to a more sustainable future. However, it can embrittle poor-quality steel materials, leading to unexpected component failures. This article looks at how materials certificates can protect OEMs from such problems.
Hydrogen is highly flammable – more so than regular fuel – and is harder to contain than oil due to its small particle size which brings understandable safety concerns. Fittings used in Hydrogen production, Hydrogen fuel cells and refueling stations must meet key performance criteria to ensure safety, reliability, and performance in application.
White Paper
This guide aims to provide engineers and end-users with an overview of the key factors to consider when specifying, building, and installing small bore tubing systems for hydrogen. It examines small bore valves, tubing, and fittings utilised in hydrogen systems, focusing on pressure ranges from vacuum to over 1,000 bar (14,500 psi).
White Paper
We focus on supporting our customers through every step of their bonding process. Our teams will go on-site for technical service, troubleshooting and process optimization.
The use of Parker EC-79 Certified fittings for hydrogen applications, alongside close collaboration with OEM ULEMCo and a local Partner is helping to pioneer technology that allows commercial vehicle fleet owners to include hydrogen among their running fuels. Taking advantage of zero-emission hydrogen fuel supports wider strategies to reduce transport-related carbon footprint.
Video
Learn how Parker A-LOK® double ferrule fittings are EC-79 Certified for use on-board hydrogen powered vehicles
Brochure
An overview of Parker fluid system technology for Hydrogen powered vehicles
Brochure
Components and systems manufactured by Parker for use with gaseous and liquid Hydrogen in infrastructure and on-vehicle applications
1005 A Cleaner Way
Huntsville, AL 35805
Tel: 256.881.2040
Riverside Road
Barnstaple EX31 1NP
United Kingdom
Tel. 0044 1271 313131