Hydrogen Dispensing | Parker US
Parker Image

A hydrogen station is a storage or filling station for hydrogen. The hydrogen refuelling station (HRS) will boost hydrogen gas from various sources to pressures required in the transportation sector – either 350 barg (5,000 psi) or 700 barg (10,000 psi).

Hydrogen Refueling Stations

Hydrogen refueling stations are pivotal in advancing cleaner energy alternatives, significantly reducing carbon emissions. By offering efficient fueling solutions for a variety of hydrogen fuel cell electric vehicles (FCEVs) such as cars, trucks, buses, and trains, they facilitate a cleaner, more sustainable mode of transportation. With the market poised for rapid growth and a goal to establish 10,000 stations globally by 2030, the reliability of these stations becomes paramount.

Due to a lower energy density than traditional fuels, hydrogen must be stored at high pressures for comparable driving ranges. The high-pressure requires robust, durable equipment and infrastructure. Reliable fueling stations must maintain consistent pressure to ensure efficient fuel transfer and prevent equipment damage. The reliability is critical to safe and efficient operations as the world transitions to clean energy.

Process flow for blue hydrogen carbon capture

Webinar

Selecting the Right Components for a Hydrogen Refueling Station

Hydrogen continues to bring about new challenges. At the core of these concerns is the fact that many components used in traditional systems are not certified to handle the additional demands that hydrogen puts on fuel systems. Find out how to select the right components for a hydrogen dispenser.

Selecting the Right Components for a Hydrogen Refueling Station

Hydrogen Value Chain Interactive

Discover how Parker can help on your hydrogen journey and learn more about the products on this page with this value chain interactive.

Hydrogen Value Chain Interactive

Fluid Conveyance for Hydrogen Refueling Stations

  • The use of fluid conveyance technology in hydrogen dispensing
    Parker products are designed to withstand the pressure requirements of storage tanks and compressors to reach the required pressure of dispensing. The products are carefully engineered to provide the highest accuracy and repeatability, allowing for consistent performance and long-term reliability.

  • Featured fittings, connectors, valves, sensors and hose products
    Parker's fittings, connectors, hoses and valves play a vital role in hydrogen fuel dispensing and are made to safely transfer hydrogen gas from storage tanks to vehicles or other systems. The components are made from materials that can withstand high pressures and temperatures related to hydrogen.


Featured Fluid Conveyance Products

Sealing Technology for Hydrogen Refueling Stations

In the filling process of vehicles and other consumers or of decentralized, stationary tanks, seals are exposed to significant pressure gradients. In combination with hydrogen’s high diffusion tendency, there is a risk of seal damage due to explosive decompression. The seals used for filling purposes must be resistant to mechanical stress and deliver reliable performance even at low temperatures.

 

View Parker's featured sealing solutions below. For hydrogen systems, Parker Prädifa uses a special, intelligent seal design paired with low-permeation, mechanically robust low-temperature materials.


Featured Sealing Technology Products

Cooling Technology for Hydrogen Refueling Stations

Cooling within the HRS is critical to ensure the correct operation of the system and to cool the high pressure compressed gas to the correct temperature to enable hydrogen-powered cars to be refilled quickly. Explore Parker Hannifin's featured solutions for hydrogen refueling station cooling listed below.

Learn how Parker is purposefully leading the way in hydrogen production.