Parker to showcase technologies at SPE Offshore Europe for fuelling a carbon-zero future | Regional English sites
MEDIA CONTACT

Lisa de Beer
Public Relations EMEA
Parker Hannifin
Phone: +27 (0)11 961 0700
Email: lisa.debeer@parker.com



5th to 8th September 2023 | Hall 3, Stand 3C53 | P&J Live, Aberdeen, Scotland

 

Aberdeen, UK, 16th August 2023 – Parker Hannifin, the global leader in motion and control technologies, will showcase its latest upstream and downstream engineering solutions for land and sea installations at this year’s SPE Offshore Europe. Taking place in Aberdeen, Scotland, between 5th and 8th September, the event will be celebrating its 50th anniversary and bringing together sector solutions from its 2023 exhibitors. A selection of Parker’s products, designed to help the oil and gas sector transition to a new energy era, will be exhibited in two zones on Stand 3C53 at the event.

Zone 1 of the company’s Stand will feature products for today’s ‘here and now’ including blowout preventer (BOP) hoses, Black Eagle hoses, bent-axis motors and contamination control solutions. Zone 2 will focus on tomorrow’s ‘tech for a cleaner future,’ including high-pressure hydrogen hoses and fittings, process filtration, Phastite tube connectors and F37 non-weld piping solutions.

Black Eagle hose

Among the product highlights in Zone 1 will be Parker’s Black Eagle range of large-bore, flexible, high-pressure, thermoplastic, wire-reinforced hoses, designed for use in upstream oil and gas applications. The hoses feature a nylon core tube with high-tensile steel wire reinforcement, and a dual-layer polyurethane outer jacket incorporating ColorGard technology. ColorGard acts as an ‘early warning’ indicator to alert end users to any excessive external abrasion that has potentially compromised the operational integrity of a hose assembly.

Hydrogen Hose 2440P-04V32

Within Zone 2, visitors will find Parker’s 2440P-04V32 hydrogen hoses on display that were developed to meet the high demands of hydrogen refuelling at 875 bar with pre-cooled hydrogen of -40°C. These reinforced hoses have a robust, kink-resistant design that offers excellent reliability and an extended life cycle. The ability to create tight-radius bends without kinking enables more convenient usage and installation in tight or limited spaces. This hose is ideal for fast refuelling operations and has a H70 pressure class.

Phastite Tube Connectors

Also part of the ‘tech for a cleaner future’ products in Zone 2, Parker will exhibit its Phastite tube connectors that are a type of ferrule-less, push-fit tube connection system. Their unique design eliminates costly welding and combines quick installation with a single assembly process to achieve a tube connector that can be used in applications up to 1,550 bar and temperatures ranging from -45°C to 93°C. Phastite is already being used on thousands of applications worldwide and, coupled with its mandatory Small Bore Expert (SBEx) training, users can make their processes smarter, faster, cleaner, and safer.

To discover more and book a one-to-one meeting with a Parker expert at the show, visit Parker’s event page: www.parker.com/gb/en/about-parker/newsroom/event-details/SPE-Offshore-Europe.html

 

About Parker Hannifin

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.