Parker Hannifin introduces innovative I/O option card to enhance servo drive performance | MSGE I/O Option Card for Parker Servo Drives
MSGE I/O Option Card for Parker Servo Drives

For further information, please visit: www.parker.com

MEDIA CONTACTS
 

Markus Gugel
Product Manager – Servo Drives
Electric Motion & Pneumatic Division
Parker Hannifin
Email: markus.gugel@parker.com

 

Lisa de Beer
Public Relations EMEA
Parker Hannifin
Phone: +27 (0)11 961 0700
Email: lisa.debeer@parker.com

Offenburg, Germany, 30th April 2024 – Parker Hannifin, the global leader in motion and control technologies, has enhanced its standalone and multi-axis Parker servo drives (PSD) offering with a new I/O option board. This versatile option card, accommodating one or two cards per drive, introduces an array of technical features that improve the adaptability and performance of the complete PSD family.

 

From motion control for axis interpolation to adapting different setpoint sources, such as speed or current commands, the optional I/O card addresses a variety of applications. It also supports encoder simulation, step and direction input.

 

Use of the I/O card has a range of benefits, including flexibility and cost-effectiveness. Furthermore, it provides a wider choice of sensors, allowing cost savings by utilizing sensors with standard interfaces instead of typically more expensive sensors with fieldbus interfaces. Directly connected sensors result in faster cycle times and reduced delays, enhancing the performance of closed-loop controls. In addition, small applications can be realized without the need for an external programmable logic controller (PLC), simplifying the overall system design.

 

Compatible with all PSD1 ranges, the I/O option card has a flexible design with one or two cards per drive. It features one encoder interface for input/emulation, eight switchable digital inputs/outputs, and four analog inputs.

 

This new I/O option card increases the potential applications of Parker servo drives, making them suitable for an extensive range of uses as decentralized control systems with motion control and PLC function in the drive. The diverse inputs and outputs facilitate direct connections to sensors, enabling internal load control or serving as setpoint inputs for current or velocity.

 

“The introduction of our I/O option card represents a significant step forward in the capabilities of our PSD1 servo drives, offering our customers greater flexibility, cost-effectiveness, and performance," said Markus Gugel, Product Manager Servo Drives, Electric Motion and Pneumatic Division.

 

This latest enhancement reaffirms Parker Hannifin's dedication to delivering solutions that empower businesses across diverse industries. The I/O option card is available now, opening a new era of possibilities for motion control applications.

 

For further information, please visit: www.parker.com

 

 

About Electric Motion & Pneumatic Division
Parker Electric Motion and Pneumatic Division is part of the Parker Hannifin Corporation Motion Systems Group and designs, manufactures and supports a full line of mobile motors and inverters, cylinders, actuators, pneumatic valves, air preparation components, servo drives, servo motors and AC/DC variable speed drives. These products are designed to improve performance, efficiency, and safety in various industrial applications as well as mobile electrification. Electric Motion and Pneumatic Division is committed to providing solutions that help customers to reduce energy consumption, increase productivity and enhance the reliability of their systems.

 

About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin