Learn more about CHO-MUTE 9009 at: CHO-MUTE 9009 Microwave Absorber Material
Melanie French
Marketing Communications Manager
Phone +44 (0) 1494 455447
Email: mfrench@parker.com
CHO-MUTE™ 9009 from Parker Chomerics is ideal for ADAS protection
High Wycombe, Bucks, UK, 31st October 2023 – The Chomerics Division of Parker Hannifin, the global leader in motion and control technologies, is introducing its CHO-MUTE 9009 microwave absorber material. Comprising a silicone elastomer matrix with a carbon filler, the material offers RF absorption performance at a high frequency range. For instance, CHO-MUTE 9009 can achieve 50 dB/cm of absorption at 77 GHz, a standard frequency used in the automotive industry for applications such as ADAS (advanced driver assistance system).
CHO-MUTE 9009 not only provides a user-friendly approach to the reduction of undesirable electromagnetic radiation from electronic equipment, it also minimises cavity-to-cavity cross coupling and microwave cavity resonances. Aside from the automotive industry, further sectors able to take advantage of this innovative absorber material include military/commercial radar, telecommunications equipment and general RF testing.
By reducing unwanted electromagnetic radiation through the absorption of signals and reduction of reflections from metallic surfaces, CHO-MUTE 9009 is suitable for use in close quarters with electronic circuitry. The material offers electrical properties that include: a surface resistance of >1M Ω/square (CEPS-002 test method); bulk volume resistivity of >1M Ω-cm (CEPS-002); 1.05 magnetic permeability (ASTM D2520); 0.001 magnetic loss tangent (ASTM D2520); electric permittivity of 10 (ASTM D2520); and 0.08 dielectric loss tangent (ASTM D2520).
CHO-MUTE 9009 is available as sheet stock at a selection of standard thicknesses with or without electrically conductive pressure-sensitive adhesive (PSA). A wide variety of fabricating techniques are also available for custom part manufacturing, including moulded profiles or die-cut/waterjet-cut (no abrasive) shapes. CHO-MUTE 9009 material is flexible, making it easy to cut and convert for use in the empirical testing of absorption solutions.
Learn more about CHO-MUTE 9009 at: CHO-MUTE 9009 Microwave Absorber Material
About Chomerics
Chomerics is a division of Parker Hannifin Corporation and is part of the Engineered Materials Group. It is the global leader in development and application of electrically and thermally conductive materials in electronics, transportation and alternative energy systems. For details, please visit www.parker.com/chomerics
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.