Parker’s new disengageable twin flow truck pump offers fuel savings and reduced life cycle costs | Regional English sites

Parker’s new disengageable twin flow truck pump offers fuel savings and reduced life cycle costs

Trollhättan, Sweden, 27. April 2023 - The Pump & Motor Division Europe of Parker Hannifin, the global leader in motion and control technologies, has announced the launch of its new disengageable twin flow truck pump, the F4 series, as an innovation for the mobile hydraulics market.

The new F4 hydraulic pump merges technology from the successful F2 twin flow pump and F3 axial piston fixed pump series, resulting in a simple and flexible solution for any vehicle requiring separate flows of differing capacities. This will have multiple applications in vehicles such as salt spreaders, hook loaders, forestry cranes, sewage trucks, snow ploughs and many others.

The patented clutch function lets the user engage and disengage the pump from the diesel engine on the move, without turning the engine off, by pressing a switch on the dashboard. This enables substantial fuel savings and a significant reduction in CO2 emissions.

If, for example, a truck (with a hook loader and a detachable snow plough) that utilizes the new F4 series pump runs for 260 hours in its first month using power take-off (PTO) for just 56 of those hours, around 1.2 kW per hour less power is required when the pump is disconnected. This equates to about 50 liters less fuel needed in that month alone, and in a year, the possible savings could exceed 600 liters (especially where the snow plough is in use only for a few of those months). The CO2 emissions are therefore also reduced by around 1.8 tonnes.

In addition, the clutch feature reduces wear and tear on the pump and minimises the risk of costly downtime and standstills, while also reducing the noise emission levels.

“The ability to disengage a twin flow pump is a huge money saver in terms of fuel savings and less wear on the pump. In the situation of a hydraulic hose failure, users also would be able drive to the workshop instead of the truck being towed, resulting in less downtime,” stated Anders Larsson, Product Leader at Pump & Motor Division Europe.

Learn more about the F4 pump series at: https://ph.parker.com/gb/en/axial-piston-fixed-pumps-series-f4

About Pump & Motor Division Europe

Parker Pump & Motor Division Europe (PMDE) constantly strives to find new solutions that can help customers build better and more productive machines. With this mission in mind, PMDE designed the Customer Service Program to supply customers with the right system or component at the right time - no matter whether working directly with Parker, or with one of its premier distributors. (www.parker.com/PMDE)


About Parker

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

 

###

Contacts:

Anders Larsson
Product Leader
Pump & Motor Division Europe
+46520404541
alarsson@parker.com

Lisa de Beer
Marcom Leader - UK & IrelandPublic Relations EMEA
Parker Hannifin
+27 (0)11 961 0700
lisa.debeer@parker.com