Parker introduces DFplus® Generation IV proportional valves for demanding industrial applications | Parker introduces DFplus® Generation IV proportional valves
MEDIA CONTACTS
 

Frank Henschke
Product Manager – Proportional Valves
Parker Hannifin – Industrial Systems Division Europe
Phone: +49 (0)2131 513-117
Email: frank.henschke@parker.com
www.parker.com/msge

 

Lisa de Beer
Public Relations EMEA
Parker Hannifin
Phone: +27 (0)11 961 0700
Email: lisa.debeer@parker.com

Kaarst, Germany, 21st. May 2024 – Parker Hannifin, the global leader in motion and control technologies, is launching the new generation of DFplus® proportional valves. The valve electronics have been fundamentally revised, opening up new possibilities for communication with the valve as well as connectivity for demanding industrial applications. The mechanical part with its patented voice coil drive (VCD), the basis for the established performance of the previous generations of DFplus valves, remains almost unchanged.

 

A new dual core processor, in the Generation IV valves, enables them to run at maximum performance level and to communicate with the PLC at the same time. The retention of the analogue command signal in combination with the use of the valve's IO-Link connection for communication is unique.

 

“The enhanced features of the Generation IV will make our DFplus valves market leaders not only in terms of dynamics and flow. They now also offer the easiest way to enter Industry 4.0 without high investments and without changing the machine control strategy”, says Frank Henschke, Product Manager Proportional Valves at Parker’s Industrial Systems Division Europe.

 

There are more innovations that provide added value. One of these new features is an integrated near-field communication (NFC) chip that allows users to obtain all status information in the field or in service situations – even when the valve is not actively powered. A 360° LED at the top of the electronics box ensures that the basic status data is immediately visible in the application by different colours or flashing frequencies. Parker’s ProPxD parameterizing software has been fundamentally revised along with an improved oscilloscope function, permitting adjustment to the application-specific parameters quickly and easily.

 

The new electronics are perfectly complemented by the mechanical characteristics of the DFplus® valves. The unique VCD with its highest resolution integrated linear variable differential transformer (LVDT) provides elevated force drive without the need of strong active return springs, resulting in real servo valve performance. Together with the high robustness, which has been proven by vibration tests with up to 60 g and 10 billion endurance test cycles, the valves have already demonstrated their suitability for numerous demanding applications.

 

With the innovations of DFplus Generation IV, Parker is ideally positioned for working with engineers facing the challenges of the future in industrial hydraulics, in particular the increasing digitalization of processes. The valves are also suitable as a 1:1 replacement for DFplus Generation III valves in existing applications.

 

To learn more about this product, visit: https://ph.parker.com/gb/en/product-list/direct-operated-proportional-dc-valve-series-d1fp-d3fp

 

 

About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.