Learn more about the SOFT-SHIELD® 4840 and SOFT-SHIELD 4860 at: Electrically Conductive Foam Based Gaskets
Melanie French
Marketing Communications Manager
Phone +44 (0) 1494 455447
Email: mfrench@parker.com
Two new products specifically designed for high-volume and high-temperature applications
High Wycombe, Bucks, UK, 24th January 2024 – The Chomerics Division of Parker Hannifin, the global leader in motion and control technologies, has introduced two new versions of its market-leading SOFT-SHIELD® 4850 multi-planar electrically conductive foam EMI shielding gasket: the more cost-effective SOFT-SHIELD 4840 for high-volume grounding applications; and SOFT-SHIELD 4860, a halogen-free EMI shielding gasket for use in high-temperature systems.
SOFT-SHIELD 4840 is an electrically conductive foam used for grounding in environmentally controlled applications. The optimal dispersion of conductive silver-plated nylon fibres embedded within a low-density urethane foam matrix means this material is electrically stable over many closure cycles, experiencing a low compression set (<15%).
Offering a more cost-effective alternative for customers, SOFT-SHIELD 4840 is ideal for high-volume applications such as consumer devices and industrial electronics. It requires lower compression force but provides slightly lower conductivity (higher through resistance). The product has an operating temperature range of -40°C to +70°C.
SOFT-SHIELD 4860 is a true multi-planar electrically conductive foam for indoor applications. Based on the unique integration of electrically conductive silver-plated nylon fibres - this time dispersed in a low-density silicon foam - SOFT-SHIELD 4860 is the high-temperature, halogen-free version of SOFT-SHIELD 4850 and offers an operating temperature up to 125°C. This performance-driven EMI shielding solution is also electrically stable over many closure cycles, undergoing a low compression set of less than 10%.
Both new products offer Z-axis electrical conductivity, low closure force, non-nickel bearing material, and compliance with RoHS, REACH and UL 94-V-0. While SOFT-SHIELD 4840 offers good through-resistance of <150 mΩ, SOFT-SHIELD 4860 provides excellent through-resistance of <40 mΩ (both at 30% gasket deflection). Similarly, the typical shielding effectiveness of SOFT-SHIELD 4840 is 60 dB, while SOFT-SHIELD 4860 provides 95 dB (both from 20 MHz to 10 GHz).
Potential applications for the new products include: high-volume consumer electronic devices (SOFT-SHIELD 4840); LCD/PDP large screen televisions (SOFT-SHIELD 4860); servers, desktop PCs and laptops; I/O panels, backplanes, connectors, access panels and rectangular/square-strip gasket seals; telecom infrastructure rack and enclosure components; and applications requiring UL94 V-0 flammability rating.
Both SOFT-SHIELD 4840 and SOFT-SHIELD 4860 are available with or without a conductive pressure-sensitive adhesive (PSA) in bulk rolls, cut sheets or custom die-cut shapes.
Learn more about the SOFT-SHIELD® 4840 and SOFT-SHIELD 4860 at: Electrically Conductive Foam Based Gaskets
About Chomerics
Chomerics is a division of Parker Hannifin Corporation and is part of its Engineered Materials Group. It is the global leader in development and application of electrically and thermally conductive materials in electronics, transportation and alternative energy systems. For details, please visit www.parker.com/chomerics
About Parker Hannifin
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century, the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.