A key part of Purpose is recognizing that Parker people and technologies have a vital role to play in making the world a better place. We call it Leading with Purpose and it's one of the core ideas at the foundation of Parker's partnership with Water Mission.
Water Mission is a non-profit organization that responds to the urgent need for safe drinking water around the world in developing countries and areas impacted by natural disasters. Since 2001, the organization has used innovative technology and engineering expertise to provide access to safe water for more than four million people in 55 countries. And yet, Water Mission did not have a system for treating saltwater. In 2014, Parker and Water Mission forged a strategic partnership, in which Parker provided the organization its highest-capacity Water Purification System that could fit in a standard 20' container.
The Parker Sea Water Desalination Unit uses reverse osmosis (RO) as its method of seawater desalination. Capable of treating up to 30,000 gallons per day, the container-based system is ready to deploy wherever temporary or emergency potable water is required.
Parker water purification systems were deployed in the US following Hurricane Katrina in 2005 and in the Philippines following Typhoon Haiyan in 2013. Water Mission deployed its Parker RO Unit in Columbia, South Carolina in 2015 in the aftermath of Hurricane Joaquin.
And then, on September 1st, 2019 Hurricane Dorian hit the Bahamas as a record-breaking category 5 storm and battered the islands of Grand Bahamas and Abaco for two days before moving North. It delivered sustained 85mph winds that razed buildings and knocked out the electric infrastructure around Marsh Harbour, Abaco's largest city.
According to Red Cross, about 45% of the homes on Grand Bahama and Abaco were severely damaged or destroyed while devastating floods compromised the water supply, leaving more than 60,000 people without clean drinking water. Water Mission was there on the ground quickly with its Parker Reverse Osmosis Unit and disaster response teams to meet the needs of residents affected.
Click any of the links below to read more about how Parker is Leading with Purpose. Want to view our videos? Click here.