Parker Distributor Rotec Empowering Utilities to Achieve Net-Zero | Parker
Image: Parker Distributor Rotec Hydraulics
Rotec Hydraulics

Rotec Hydraulics Ltd, experts in system solution design, developed a pioneering electric winch system that offers a zero-emission alternative to hydraulic winches. This innovation supports their utility customer in achieving net zero goals with enhanced performance and precision.

CHALLENGE

Decarbonising Specialist Hydraulic Winch Systems

The customer, a national company working within the utilities sector, has ambitious net zero goals and Rotec Hydraulics, as its sole winch design, supply and service provider was keen to support.

 

SOLUTION

Customised Electric Winch System

An electrical winch system, utilising Parker components, that produces the same amount of power as its hydraulic equivalent, whilst meeting the client’s bespoke operational requirements, including proportional speed control and two operation modes - lift and self-recovery

 

BENEFITS

Zero Emissions, Enhanced Precision, and Reliable Performance

Rotec Hydraulics’ electric winch system reduces CO2 emissions, supporting net zero goals. The system offers controlled ascent and descent capabilities, customisable design, robust components and unlimited run time.

 

“As a key supplier and integrated partner for over 20 years, Rotec’s ability to navigate challenges is exceptional and their delivery of planned maintenance is consistently excellent.” 

 

 Fleet Technical Specialist, Utility Company

Parker Distributor HydSupply solving a customer's hydraulics challenge

 

Showcasing Parker Distributors’ Expertise in Innovative System Design

Rotec Hydraulics, a certified Parker distributor located in the UK, has innovatively designed and developed the first-of-its-kind electric winch system in response to a request from a client. The customer, a national company working within the utilities sector, has ambitious net zero goals and Rotec, as its sole winch design, supply and service provider was keen to support.

Expertise in system solution design

Rotec’s in-house design team embarked upon a R&D project specifically dedicated to produce an electric winch with the equivalent performance and functionality of the hydraulic winch that the client currently uses on their 500 strong fleet of Isuzu D-Max vehicles.

Stepping up the design challenge

Despite other winch providers saying an electric winch system capable of proportional speed control lifting 1.5 tons and dragging 3.6 tonnes and not overheating was impossible, Rotec are pleased to reveal their new offer to the market.

This particular example features two operational modes (lifting and pulling). The proportional speed control allows for safe, controlled ascent and descent of the winch system when lifting. Operators have reported that the infinite winch speed control using joysticks in cab and/or remote pendant have allowed for more precise and accurate placing of the load than the previous hydraulic winch delivered.

The integrated thermal management of both motor and motor inverter along with natural air cooling of the motor inverter, means that Rotec’s electric winch system has an unlimited run time.

The electric winch system is fully customisable and Rotec is keen to support their client with electrifying all of their winch systems, including those fitted to MAN lorries and Marooka tracked dumpers.

Sustainability

Rotec’s electrical winch system reduces CO2 emissions as a result of being powered by a lithium battery, rather than the vehicle’s diesel engine.  The vehicle engine does not need to be turned on in order to operate the winch, unlike its hydraulic counterpart. 

The electric winch’s carbon emissions are minimised with the only emissions being those generated when the vehicle is in motion and it is charging the winch system’s lithium battery.

Not just a supplier of parts

As demonstrated in this case, Parker Distributors are not just suppliers and stockists of parts but can provide system solution design to meet your specific needs.

Winner of Manufacturer of the Year 2023 at the Somerset Business Awards, Rotec can provide tailored winch system designs and offers design, manufacture, fitting and on-site servicing and repair service backed with excellent customer service. 

Customers can customise rated line pull, line speed or rope type and capacity to optimise their operations. High quality, robust components mean all Rotec winch systems are suitable for operating in challenging environments.

Rotec’s innovative electric winch system has enabled its customer to not only cut emissions but work smarter, more accurately and increase productivity with proportional control capability and/or remote monitoring options.

 

“This project is an example of how Rotec Hydraulics is spearheading electrification within the fluid power industry to enable decarbonisation of the hardest-to-abate industry sectors.

 

The addition of Parker components, including IQAN technology, has made the challenge of producing the same, if not enhanced, performance compared to the equivalent hydraulic winch system solution possible.”

 

Paul Prouse, Managing Director of Rotec Hydraulics Ltd.

Rotec Hydraulics is a Parker Certified Distributor, based in the UK specialising in providing quality design, build, installation and maintenance of hydraulic, pneumatic and electrical mechanical systems.