Over recent years, environmental concerns have led to pollution reduction legislation and a growth in the electrification of mobile machinery. At the same time, rising cost pressures are driving OEMs to seek design solutions that maximise performance and minimise total cost of ownership. Focusing on hydraulic tank optimisation can offer many benefits to help solve these challenges:
Watch an interview with our tank optimisation experts to learn more
A footprint reduction of up to 75 L per machine frees up space for battery installation enabling electrification technologies.
A reduction in the weight of the hydraulic reservoir by up to 100 kg decreases fuel consumption and carbon dioxide emissions.
A smaller tank reduces steel and hydraulic oil demand decreasing manufactring costs by up to €1,000,000 per machine series per year.
A smaller hydraulic tank requires less oil so disposal can be reduced by up to 500,000 L per machine series per year.
Take a sneak peek at Parker's R&D facilities. Learn how we work with you to improve the design of the hydraulic reservoir from computer simulations to laboratory and on-site testing.
We work with you from concept to design to speed up your development time
STEP 1
Parker’s engineers have decades of experience in hydraulic filtration and tank optimisation. We work closely with your engineering team, from concept to final design, to create a total system solution. This approach reduces your development time and brings your innovations to market faster.
Our team of experts will work with you to identify key objectives, whether it be tank size reduction, removal of air, heat dissipation or improvement of flow streamlines. We study your system, analyse your CAD models to identify locations of filters and any baffle plates, any suctions and flow rates involved.
STEP 2
After an initial consultation to understand your system, Parker will use computation fluid dynamics (CFD) to simulate the current performance of your hydraulic reservoir. CFD can determine oil flow streamlines, oil and air phase fractions in the tank, heat distribution and oil properties. The effectiveness of the internal components and flow path to the suction line(s) are then investigated to identify:
STEP 3
After the completion of the simulations a physical tank will be tested at our hydraulic filtration site in Urjala, Finland, to confirm that the performance of the reservoir matches the simulation results.
By using the Oilpas test unit we can determine air in oil contamination by measuring the quantity of and size of air bubbles. Besides the air in oil testing we also visually observe the behaviour of the air bubbles.
After the physical tank testing the reservoir design can be finalised for series production.
STEP 4
The final step of the tank optimisation program will be on-site testing to test the performance of the hydraulic tank on the equipment. By installing the Oilpass test unit we can measure the quantity of and size of air bubbles during real operating conditions.
Other tests can be done simultaneously to get a better understanding about performance of the full hydraulic system.
Parker’s team of hydraulic experts worked with Volvo Construction Equipment when developing their new F series excavator. When designing their new model, they wanted to increase the cab size to improve the operator experience. They also wanted to develop an optimised hydraulic tank that was suitable for all of their models from the F series platform. This would allow them to standardise the assembly and minimise the number of parts in production, effectively reducing their tooling costs.
Parker worked closely with Volvo to develop an integrated solution, designed to minimise the hydraulic tank volume.
Selecting the correct top tank filter: The iProtect® GLF Filter Series was chosen as it provides in-to-out filtration to allow a safer and cleaner filter element replacement. The iProtect® GLF Filter Series also provides more filtration media surface, reducing flow velocity and oil foaming via the diffuser.
Hydraulic reservoir performance simulation: Parker used computational fluid dynamics (CFD) to ensure space inside the tank was optimised. David Lazzaro, Lead Engineer Hydraulic, Volvo Construction Equipment commented that “it helped a lot during development as it allowed us to find the correct positioning of the diffuser and check tank deaeration without doing physical tests”. This allowed for time and money savings for tooling.
Verifying the solution: David found that “the help of Parker with the Oilpas tool was also very useful to verify all of the different assumptions taken during the CFD analysis”.
Parker hydraulic tank optimisation expert interview
Learn about the market trends driving hdyraulic tank optimisation and how Parker can work with you from concept to design to bring your innovations to market.
Parker's tank optimisation R&D facility overview
Learn how we work with you to improve the design of the hydraulic reservoir from computer simulations to laboratory and on-site testing.
Design innovation through high-fidelity simulations
Learn how parker use computer simulations to help you innovate your hydraulic tank design.
Hydraulic tank optimisation brochure
The hydarulic tank optimisation brochure is now available to download
Hydraulic reservoir optimisation
Discover how Parker used CFD to establish an optimised hydraulic tank design when challenged with improving deaeration while reducing tank size.
Tank top return line hydraulic oil filter
Filter pressure and vacuum indicator
Top-mounted breathers and filler breathers
Fluid level / temperatures gauges, float and capacitive level switches
Suction elements / inbuilt filters