For environmentally-sealed and EMI-shielded electronics devices, there is no better full-system solution than an overmolded cover. And with Parker, customers have access to a wide range of qualified, high performance elastomer materials including most Parker O-Ring compounds.
Overmolding is the process of molding a gasket directly onto a metal or composite substrate. Instead of extruded cord stock, press-in-place, or molded sheets, the elastomer gasket is bonded directly onto the housing, box, or enclosure, and will retain its shape after molding.
Top Benefits
Top benefits of using overmolded technology for enclosures include:
View the quick video highlighting the top five feature benefits of Gask-O-Seal® overmolded technology for static sealing of defense electronics enclosures.
Enclosures provide static sealing protection for electrical, electronic, or mechanical components and instruments where typical functional performance requirements may include:
Dependable sealing of enclosures that safeguard IMU's is critical for delivering highly reliable measurements in changing environments such as robotics, stabilization, and pointing applications.
Micro-electro-mechanical system (MEMs) based inertial measurement units (IMU). Miniaturization, remote data interface across various markets including ag, AUVs, industrial equipment, robotics, survey/mapping, stabilization, drone.
Also known as Attitude Reference (AR) Units, this sensor is an example of non-military applications involving roll damping, terrain compensation, and transformation between coordinate systems on platforms.
Sophisticated electronics typically associated with classified and mission critical navigation tasks requiring consistent precision for robotic, manned, and unmanned systems providing centimeter-level accuracy.
Learn about comparative advantages of different static face seal options and why you would choose over-molded technology.
As an improvement over flat gaskets and alternative to an o-ring in a groove, Gask-O-Seals provide near zero leakage sealing. Learn about feature benefits and configuration options.
Learn how overmolded bonded solutions provide greater reliability for tangential and permeation leakage protection in safeguarding electronics and critical instruments.
Our customer came to us with multiple pains related to the incumbent sealing method which utilized an O-ring. Read how worked to provide a one-piece overmolded solution to resolve their challenges.