HIGH WYCOMBE, Buckinghamshire, 23. February 2022—The latest edition of Parker Chomerics Conductive Elastomer Engineering Handbook has been updated, making it easier than ever to select the right materials and products for any EMI shielding application.
Comparing different materials and their benefits, the handbook features a quick reference guide showing common materials suitable for use in commercial and military applications. The guide lists common conductive elastomer materials together with appropriate fillers and binders for them.
It also assesses their level of shielding and corrosion resistance on aluminium and details whether the materials meet the requirements of MIL-DTL-83528.
Information on the performance of sheets and extrusions has also been updated, with new test data on compression and deflection behaviour.
Another feature is the improved part number builder for moulded parts, making it easier to build the part number for the product the Design Engineer wants.
With an extensive section on conductive elastomer gaskets, advice on selecting materials for corrosion resistance, a detailed section on physical performance and a comprehensive catalogue of Parker Chomerics products, the Engineering Handbook is a complete guide to designing Conductive Elastomer applications.
Download your free copy of the Conductive Elastomer Engineering Handbook here: Engineering Handbook
Hard copies are also available to engineers based in Europe.
Chomerics is a division of Parker Hannifin Corporation and is part of its Engineered Materials Group. It is the global leader in development and application of electrically and thermally conductive materials in electronics, transportation and alternative energy systems. For details, please visit www.parker.com/chomerics
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###
Melanie French
Marketing Communications Manager
Phone: +44 (0) 1494 455447
Email: mfrench@parker.com