COLOMBES, France, 17. January 2022—Parker Hannifin, the global leader in motion and control technologies, is introducing a new safety block (SB series) for hydraulic accumulators that simplifies the selection, installation and maintenance process of these important system components. Due to the broad variety of accumulator types and their applications, the market is proliferated with an equally wide expanse of safety blocks that, until now, has made selection challenging for many customers. Developed by the company’s Cylinder and Accumulator Division Europe (CADE), the new safety block overcomes this time-consuming issue.
Safety blocks enable hydraulic accumulators to be isolated for maintenance work, repairs or system tests, acting as an emergency shut-off device to protect against system failure. Based on the ethos that simple engineering makes for a safer solution, the versatile SB series offers full functionality in a single product: isolation, drain, peak pressure protection and pressure control. As a result, choosing the right safety block is now far easier – regardless of the application. Typical markets set to benefit from the new concept include industrial, mobile, oil and gas to list but a few.
Offering an improved design that helps to minimise space requirements and to ease installation, the SB series is available in sizes 10, 20 and 32. Users can enjoy advantages such as a standardised temperature range of -20°C to 80°C, and high corrosion resistance compliant with ISO 9227. In addition, the SB series is PED-certified and suitable for use in ATEX environments (manual version only).
Ideal for all bladder, diaphragm and piston-type accumulators, customers can select from models with electric or manual relief valves. The SB series features either a BSPP or SAE accumulator connection, with size 32 offering an SAE accumulator connection as standard. Furthermore, size 32 offers the choice of flanged or threaded hydraulic connection. A variety of voltage options (24VDC, 110/120VAC, 230VAC) ensure the SB range is suitable for all types of industrial applications, with the pressure range corresponding to the accumulator operating pressure (up to 350 bar).
Says Laurent Nauroy, product manager at CADE: "Our customers have repeatedly asked for a simplification of the previous series. The new SB safety block is the result of this feedback. Our SB series allows for simple design, simple engineering and simple selection."
As standard, Parker Hannifin supplies its SB series safety blocks without an adapter.
"The concept of accumulators without adapters is based on the desire of our customers to complement an accumulator safety block with different adapters to suit the specific application,” states Nauroy. “This creates more flexibility at lower cost.”
For more information and to configure application-specific safety blocks, please visit: https://ph.parker.com/gb/en/sb-safety-block
With over 50 years of experience, we have worked with customers from a diverse range of markets and applications which has enabled us to gain extensive knowledge and expertise in accumulator, cooler and cylinder technologies. We often work closely with our customers to provide solutions for hydraulic systems. Our product range helps customers to enhance the longevity of their parts and systems whilst also improving efficiency and output. Offering a comprehensive range accumulators, coolers and cylinders we can supply products to suit any requirement, for any geographic location.
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###
Simone Joseph
Simone.joseph@parker.com