LANCASTER, NY, May 12, 2021—The Industrial Gas Filtration and Generation Division of Parker Hannifin Corporation, the global leader in motion and control technologies, today announced the launch of its new Parker PPD Series Portable Desiccant Compressed Air Dryers and ROVR Oil Vapor Removal System, designed to deliver ‘technically’ oil-free compressed air for the rental industry.
Parker’s PPD Series Portable Desiccant Compressed Air Dryers
Parker’s new PPD Series is a range of comprehensive compressed air treatment systems each equipped with multiple stages of a filtration, a twin tower adsorption (desiccant) dryer, optional integrated aftercooler and water separator package and an industry-leading Programmable Logic Controller (PLC). Packaged on a portable, heavy-duty skid, these highly engineered systems ensure high quality compressed air in accordance with ISO8573-1, the international standard for compressed air quality.
To achieve the stringent air quality levels required for today’s modern production facilities, a careful approach to system design, commissioning and operation must be employed. Compressed air treatment using just one purification technology or at one point in the compressed air system is not enough to achieve high purity levels defined by ISO8573-1. Multiple stages of purification should be utilized to ensure the most effective solution for high quality compressed air.
To guarantee maximum performance and reliability, Parker’s PPD Series portable desiccant compressed air dryers are comprehensive filtration and dehumidification systems that protect the entire compressed air network, providing the best quality compressed air, exactly where it is needed.
Parker’s ROVR Oil Vapor Removal System
Parker’s new ROVR-1600A is an oil vapor removal system designed to deliver compressed air in accordance with ISO8573-1 Class 0 for Total Oil when installed downstream of a portable desiccant compressed air dryer and filtration system.
The ROVR-1600A is a cartridge-based filtration system that is designed, tested and third-party performance certified to reduce oil vapor down to ≤ 0.003 mg/m3. This adsorption filtration system pairs easily with any of Parker’s PPD Series dryers (≤ 1600 scfm) to deliver ‘Technically Oil Free Compressed Air’ from either oil-free or oil-lubricated compressors.
For more information or for assistance with sizing and quoting, please contact the Parker IGFG Applications Engineering team at FAFquotes@parker.com.
Parker Hannifin’s IGFG Division protects and purifies using diverse solutions engineered for the customer's unique application. We are the filtration resource for customers backed by state-of-the-art labs and advanced filtration research, world-class manufacturing processes, and application engineering experience for any filtration challenge.
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###
Randy Peccia
Parker Industrial Gas Filtration & Generation Division
(800) 343-4048
randy.peccia@parker.com