Parker Autoclave Engineers needle valves and fittings receive EC-79 certification | Regional English sites

BARNSTAPLE, United Kingdom, 4. July 2022—Parker Hannifin, the global leader in motion and control technologies, has received EC-79 certification for its Autoclave Engineers SM Series of medium-pressure needle valves, and its medium-pressure cone and thread fittings. The EC-79 approval and certification are part of an EU regulation requirement for components and systems that are intended for installation on hydrogen-powered vehicles.

The need for more sustainable, energy-efficient vehicles that release zero pollution, i.e. emission of water vapor instead of CO2 into the atmosphere, is steadily on the rise. Parker is supporting the global decarbonisation efforts through a broad range of solutions enabling safe and efficient operation for a variety of hydrogen applications.

EC-79 type-approval certifies components used can withstand electrical, mechanical, thermal and chemical operating conditions without leaking or becoming deformed. It also ensures components can reliably withstand expected temperatures and pressures during their lifetime and are designed in such a way that they can be installed and protected against damage. Parker’s products underwent a series of vigorous testing to ensure they meet the stringent qualification of the regulation.

The hydrogen variation to the needle valves incorporates a unique stem/seat and PTFE packing design that can withstand temperatures ranging between -40°C and 120°C and pressures of up to 700 bar (10,152 psi). Both the SM Series needle valves and cone and thread fittings are available with anti-vibration connections, which move stress concentration to the unthreaded part of the tubing, and are supplied in sizes up to 1 inch.

Franck Grignola, Product Manager for Parker Instrumentation Products Division Europe, comments: “EC-79 certification is proof of the high quality of Parker Autoclave Engineers’ range. Parker easily passed all the tests for this qualification with success, which is not surprising due to the quality of the product ranges and expertise of Parker’s engineering team.”

These Parker Autoclave Engineers valves and fittings complement the already EC-79-certified range of A-LOK® two ferrule tube fittings, which were designed to achieve quality leak-free connections on-board hydrogen-powered vehicles, up to 350 bar pressures and for temperatures down to -40°C. These fittings provide reliable operation in cryogenic, pressure & thermal cycling, and vibration applications. Other products within Parker’s instrumentation range suitable for hydrogen applications include fittings, tubing, filters, ball valves and check valves, as well as a range of cryogenic valves suitable for liquid hydrogen applications.

For more information about how Parker Hannifin is supporting the energy transition and safe deployment of hydrogen as an environmentally friendly alternative fuel source, please visit: http://www.parker.com/hydrogen-service.


About Parker Autoclave Engineers

Parker Autoclave Engineers, part of Instrumentation Group of Parker Hannifin, are worldwide experts in the design and production of high-pressure valves, fittings, and tubing. With pressures up to 150,000 psi (over 1000 MPa), the range of products are first choice for the petrochemical, chemical, water blast, water jet, and oil and gas industries. For more information visit www.parker.com/ipd or www.autoclave.com.
 

About Parker

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

###

MEDIA CONTACT

Franck Grignola
Product Manager, Parker Autoclave Engineers – Europe
+44 (0) 1271 31313
 franck.grignola@parker.com