Parker Expands Thermal Interface Materials Offering | Regional English sites

HIGH WYCOMBE, Bucks, 5th May 2021—The Chomerics division of Parker Hannifin Corporation, the global leader in motion and control technologies, today announced the launch of THERM-A-GAP GEL 75, a 7.5 W/m-K single component dispensable thermal interface material designed for high performance applications.

THERM-A-GAP GEL 75 is a single component, gel material best suited for today’s high-powered electronics applications. When applied to a heat generating component, THERM-A-GAP GEL 75 provides minimal stress and pressure due to its low compression force and represents the highest thermal conductivity dispensable available from Parker Chomerics. Its flow rate is nearly 3x faster than the next closest performing material in the THERM-A-GAP family.

THERM-A-GAP GEL 75 is best suited for high volume, automated production, specifically found in telecommunications equipment, automotive safety electronics modules, power supplies, and memory and power modules.

The opportunity for automation is a significant advantage for THERM-A-GAP GEL 75 over thermal gap pads because gel dispensing systems allow for support of multiple size and thickness requirements with a single system configuration. While thermal gap pad placement can be automated to an extent, the equipment and fixturing required to do so is typically quite specialised and may not be readily adapted from one job to another.

“GEL 75 was formulated to accommodate the future high-power demands of many different markets, including 5G enabled telecom infrastructure, automotive applications -- any application that is seeing increased bandwidth demands that generate excessive heat.” says Brian Mahoney, Global Thermal Business Unit Manager, Parker Chomerics. “It is the next evolution in our THERM-A-GAP gap filler family of easy to use, reliable, high performance, single component dispensable gels.

THERM-A-GAP GEL 75 is now available globally in different sizes of syringes, cartridges, and pails to suit a wide variety of customer needs. Learn more about THERM-A-GAP GEL 75 and the THERM-A-GAP family of products at www.parker.com/chomerics .


About Chomerics

Chomerics is a division of Parker Hannifin Corporation and is part of the Engineered Materials Group. It is the global leader in development and application of electrically and thermally conductive materials in electronics, transportation and alternative energy systems. For details, please visit www.parker.com/chomerics.

About Parker

Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.

###

MEDIA CONTACT

Melanie French
Marketing Communications Manager
+44 (0) 1494 455447
mfrench@parker.com

Jarrod Cohen
Marketing Communications Manager
Chomerics Division Europe, Engineered Materials Group
+1 339 227 0703
jarrod.cohen@parker.com