CARSON, CA, April 8th, 2021—The Water Purification Division of Parker Hannifin Corporation, the global leader in motion and control technologies, today announced the release of its next generation of seawater systems, the H2O Eco, adding to the suite of “Patent Pending” energy recovery system.
The H2O ECO features a compact machine completely enclosed in an aluminum frame, and offers potable water safe for drinking and cooking. The H2O ECO is an extremely quiet, compact water maker for leisure marine applications and serves as the perfect seaworthy companion for anyone seeking a low power consumption watermaker.
“The new H2O Eco uses patent-pending energy recovery technology that can provide up to 14.2% potable water production from any feed source” said Paul Kamel, product manager, Water Purification Division. “We are excited to add this new, highly reliable technology to our family of watermakers.”
With a compact design frame that enables boat owners to fit their watermaker into tight spaces, the H2O Eco is perfectly suited for small to mid-sized power conscious vessels or catamarans. The H20 Eco is available in 400 to 600 gallon per day capacities.
Learn more about the H2O ECO at H2O ECO.
Parker Water Purification is the leading provider of reverse osmosis desalination plants serving the marine markets and is dedicated to serving the needs of all mariners in Leisure Marine, the Coast Guard, the US Navy, Foreign Navies, Commercial Marine, Disaster Recovery, and Offshore Oil & Gas with over 100 years of combined experience. Visit www.parker.com/waterpurification to learn more.
Parker Hannifin is a Fortune 250 global leader in motion and control technologies. For more than a century the company has been enabling engineering breakthroughs that lead to a better tomorrow. Learn more at www.parker.com or @parkerhannifin.
###
Paul Kamel
Parker Water Purification Division
310 894 4121
paul.kamel@parker.com