In green hydrogen production, electrolysis is used to break down water into its individual elements; hydrogen which is compressed and sent to storage, and oxygen which is either stored or vented to the atmosphere.
There are different electrolyzers that can be used:
- Proton Exchange Membrane (PEM) Electrolyzers
- Alkaline Electrolyzers
- Solid Oxide Electrolyzers
PEM electrolyzers use a solid polymer electrolyte that only allows hydrogen ions (protons) to pass through to form hydrogen gas on the cathode side.
Alkaline electrolyzers use an electrolyte solution (usually potassium hydroxide) which allows hydroxide ions through leaving hydrogen gas bubbles.
A solid ceramic material is used as the electrolyte at high temperature. Water is used in the form of steam which results in higher energy but produces ultra-pure hydrogen with great efficiency.
Regardless of the electrolyzer type, Parker technologies are essential to protect the process, to maintain efficiency and to purify the hydrogen gas stream to the required high standard. Parker’s broad filtration portfolio includes liquid filtration, gas separation, purification and cooling, hydraulics, fluid conveyance and sealing.
Learn how Parker is purposefully leading the way in hydrogen production.