To give you the best possible experience, this site uses cookies. By continuing to use the site, or by staying here, you agree to our use of cookies in line with our Privacy Policy. Learn more including how to manage cookies here.

Face

The cross section of the O-ring can be measured in both the axial and radial direction. A face seal uses the axial cross section, or face of the O-ring to seal.  When using an O-ring as a face seal, a groove is cut in a flat surface, such as a plate.  The O-ring is placed in the groove and a second flat surface compresses the O-ring. An O-ring in a face seal design is static, meaning that that once installed, the O-ring does not move.  While the application pressure may cause the O-ring to shift slightly, this is still considered a static seal.   Face seals can seal internal pressure, external pressure, or both.  

 

Parker Hannifin
O-Ring & Engineered Seals
2360 Palumbo Drive
Lexington, KY 40509
Ph: 859-269-2351
Fax: 859-335-5128
oesmailbox@parker.com www.parkerorings.com